Running RTCS example for MQX 4.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running RTCS example for MQX 4.1

1,323件の閲覧回数
chaitannyamahat
Contributor II

Hello Everyone,

I am using CW 10.6 and recently installed MQX 4.1 module.

Hardware : TWRK60D100M

As per the manual (which was for MQX Version 3.8).

I have imported the .wsd file and compiled the RTCS code, it generated a compressed library , rtcs.a .

Now I need an application. I imported httpsrv_twrk60d100m project. There are only source files and project files, nothing more. In the manual they have shown that there is a complete project files & the project gets compiled. In my case obvisiously the code did not get compiled.

How to compile and run the RTCS example. How to proceed further.

Regards,

Chaitannya

タグ(3)
0 件の賞賛
返信
1 返信

1,193件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Chaitannya:

I think you need to compile all libraries (psp.a, bsp.a, rtcs.a, mfs.a, shell.a) before you compile the application.


Have a nice day,
Daniel

0 件の賞賛
返信