Running RTCS example for MQX 4.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running RTCS example for MQX 4.1

1,364 Views
chaitannyamahat
Contributor II

Hello Everyone,

I am using CW 10.6 and recently installed MQX 4.1 module.

Hardware : TWRK60D100M

As per the manual (which was for MQX Version 3.8).

I have imported the .wsd file and compiled the RTCS code, it generated a compressed library , rtcs.a .

Now I need an application. I imported httpsrv_twrk60d100m project. There are only source files and project files, nothing more. In the manual they have shown that there is a complete project files & the project gets compiled. In my case obvisiously the code did not get compiled.

How to compile and run the RTCS example. How to proceed further.

Regards,

Chaitannya

Tags (3)
0 Kudos
Reply
1 Reply

1,234 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Chaitannya:

I think you need to compile all libraries (psp.a, bsp.a, rtcs.a, mfs.a, shell.a) before you compile the application.


Have a nice day,
Daniel

0 Kudos
Reply