Replacing the libraries with source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Replacing the libraries with source code

ソリューションへジャンプ
2,253件の閲覧回数
SVC2
Contributor II

Hi,

 

I am trying to compiler the web_hvac_m52259evb example without the libraries. Instead, I would like to have the source code.

 

I started with shell libraries: I removed the shell.a and replaced it with: Shell Source

 

  i.e.,

            Shell Source\MQX

            Shell Source\Shell

            Shell Source\MFC

            Shell Source\RTCS

 

I get a compiling/linker error:

                shell_flush_cache is defined in sh_cash.c and sh_flush.c.

Similarly,

                Telnetd_shell_template defined in RTCS.c and sh_tnetd.c

 

The function and structure are defined in 2 files and there seem to be no #ifdef dictating which one to use.

 

So which one should I use and why?

 

Thanks,

S

 

0 件の賞賛
返信
1 解決策
2,081件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi,

 

there shouldn't be any difficulties in using source code instead of libraries (although I also do not see much advantages).

 

The first problem :

shell_flush_cache - this function is defined in both files, but only one file is really used in shell project. Use the one which you find in shell library.

 

Telnetd_shell_template - this is different, the linker automatically override the function definition from library by the one defined in application. In your case - having both files in one project you should delete/rename one of them.

 

PetrL

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,082件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi,

 

there shouldn't be any difficulties in using source code instead of libraries (although I also do not see much advantages).

 

The first problem :

shell_flush_cache - this function is defined in both files, but only one file is really used in shell project. Use the one which you find in shell library.

 

Telnetd_shell_template - this is different, the linker automatically override the function definition from library by the one defined in application. In your case - having both files in one project you should delete/rename one of them.

 

PetrL

0 件の賞賛
返信