Hi All,
I am using mqx v4.0 and of code warrior v10.2 and have created one project which is receiving request of html page.Problem is there are upto 23 variable which i need to check and send via module,but for loop is not working means module is not sending that data.I also have attached the code with this.Please send me solution. Variable are individually checked and module is sending data but in for loop it is not working.Plz Help.........
Note:
Here in for loop "i" of cgi.c is indicating name of variables in index.html page.
Original Attachment has been moved to: cgi.h.zip
Original Attachment has been moved to: index.html.zip
已解决! 转到解答。
Hi Utsavi,
web_hvac example uses multiple variables. have you checked this example?
Regards,
Carlos
Hi Carlos,
Thnx for reply.
Of course I have seen that and from it I have made my project by taking
some portion of that demo.
The variable that is used in web_hvac demo is of small number.
If I want to use say 100 variable start form name="0" upto name="99" then I
need to use "for loop" with httpd_get_varval,but it was not working.Right
now I have made the code for that and it is working well..
Thnx again for reply......:smileylaugh::smileyhappy:
On Thu, May 29, 2014 at 8:33 PM, Carlos Alberto Musich Cuevas <