RTOS for MPC5606B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTOS for MPC5606B

1,719 Views
abhishekabhi
Contributor I

Is it possible to use MQX with Qorivva processors(MPC5606B)?If the MQX RTOS cannot be used is there a low-cost or free RTOS that anyone has used with the Qorivva?

2 Replies

1,520 Views
RadekS
NXP Employee
NXP Employee

Unfortunately MPC5606B isn’t directly supported by any MQX release.

You have to create your own port to this MCU (at least BSP) or ask (and pay) for such service.

Most similar supported part (in MQX4.1) is PXD10.

You can use MQX level 2 Support:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX_SUPPORT

Or Professional Engineering Services:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_PROFESSIONAL

Note: MPC5668G is ekvivalent of PXN20 series


Best Regards,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,520 Views
ashbc1
Contributor III

We run an MQX port on an MPC5668G.  We have had issues but they have turned out not to be MQX.  I don't know your exact processor but I can't see why it wouldn't port