RTOS Programming on K60 mC, using KSDK - MQX RTOS "TWR-K60D100M"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTOS Programming on K60 mC, using KSDK - MQX RTOS "TWR-K60D100M"

Jump to solution
2,608 Views
abhishekinamdar
Contributor II

Hello

     I 'm planning to use "TWR-K60D100M" microcontroller for RTOS programming, using KSDK and MQX RTOS. Can you give Step by Step procedure for the installation of " Kinetics Design Studio IDE" or KSDK with MQX RTOS Module.

Regards

Abhishek

Tags (1)
0 Kudos
Reply
1 Solution
2,233 Views
DavidS
NXP Employee
NXP Employee

Hi Abhishek,

The most up-to-date KDS/KSDK have good support for both TWR-K60D100M and FRDM-KL25Z.

http://www.freescale.com/kds

http://www.freescale.com/ksdk

The MQX (and other RTOS's) can be chosen to be installed or not during the KSDK installation process.

Regards,

David

View solution in original post

0 Kudos
Reply
8 Replies
2,233 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Abhishek,


for installing KDS - Kinetis Design Studio Integrated Environment (IDE)

        and according to your platform please download the executable file.

KDS_.png

For additional information you can see documentation for KDS, be aware you install 2.0

KDS_2.png

The procedure is very easy, firstly you must accept the conditions,

KDS_a.pngkds_b.png

and that´s it. The workspace would probably be at C:\Users\<your profile>\workspace.kds and KDS folder could be here C:\Freescale\KDS_2.0.0

for installation KSDK, please visit Freescale MQX™ RTOS for Kinetis SDK|Freescale and Download it according to your platform

KSDK_MQX.png

and install it.

KSDK_1.pngKSDK_2.png

KSDK_3.pngKSDK_4.png

KSDK_5.pngKSDK_6.png

You can go back after installation and modified it, don´t worry.

I can also recommend you Getting Started with Freescale MQX RTOS for Kinetis SDK which is located after this installation at C:\Freescale\KSDK_1.1.0\rtos\mqx\doc

Let me know if the information help you,


Have a great day!


Best Regards,

Iva

0 Kudos
Reply
2,233 Views
abhishekinamdar
Contributor II

Hello Iva,

     Thanks for the replay, we did the installation of KDS IDE, KSDK and MQX RTOS (Downloaded and Installed) as in the steps mentioned above. As also did the "Help - New Software Install - Kinetis Eclipse KSDK Update(.zip file) Link:C:\Freescale\KSDK_1.1.0\tools\eclipse_update\KSDK_1.1.0_Eclipse_Update.zip). But still we don't have the option to select the "Kinetis SDK" as shown in the image below.

KSDK_PATH error.PNG.png

Regards

Abhishek

0 Kudos
Reply
2,233 Views
DavidS
NXP Employee
NXP Employee

Hi Abhishek,

Three things to try:

1) Review this post Re: I can not create a new KDS 2.0 project for MK22FN1M0xxx12 with Kinetis SDK support.

2) Did you do update of KDS using Help->Install New Software... and select Freescale KDS Update Site - http://freescale.com/lgfiles/updates/Eclipse/KDS ...then Select All and follow wizard steps ?

3) Un-installed the KSDK plug-in and re-install?  Help->About Kinetis Design Studio->Installation Details... then select the KSDK 1.1.0 Eclipse Update and click Uninstall...

Regards,

David

0 Kudos
Reply
2,233 Views
abhishekinamdar
Contributor II

     And as well, when we tried for the 3rd step you mentioned ( Un-installed the KSDK plug-in and re-install?  Help->About Kinetis Design Studio->Installation Details... then select the KSDK 1.1.0 Eclipse Update and click Uninstall.) We saw 2 version of Eclipse Update installed, 'is it fine..?' as show in the image below.

KDS_4.PNG.png

     - After selecting the old version "Eclipse Update for KSDK 1.0.0-GA" the Uninstall option is grayed off as shown in above image.

0 Kudos
Reply
2,233 Views
DavidS
NXP Employee
NXP Employee

Hi Abhishek,

Sorry for delay.

I only uninstalled the KSDK 1.1.0 Eclipse Update.  Re-started KDS and then re-installed the eclipse plug-in.

Regards,

David

0 Kudos
Reply
2,233 Views
abhishekinamdar
Contributor II

Hello David,

     Thanks for the response, we reinstalled couple of time the KSDK/MQX support was available for the K60, but same issue with KL25. I guess there will be standard procedure for the installation for the KSDK/MQX support for all the Evaluation board. Need to get in touch with the Frescale Technical team. officially.

     Due to the issue we uninstalled the Freescale KDS IDE and using CodeWarrior.

Thanks David again for the support.

Regards

Abhishek

0 Kudos
Reply
2,234 Views
DavidS
NXP Employee
NXP Employee

Hi Abhishek,

The most up-to-date KDS/KSDK have good support for both TWR-K60D100M and FRDM-KL25Z.

http://www.freescale.com/kds

http://www.freescale.com/ksdk

The MQX (and other RTOS's) can be chosen to be installed or not during the KSDK installation process.

Regards,

David

0 Kudos
Reply
2,233 Views
abhishekinamdar
Contributor II

Hello David,

We tried all the three methods mentioned by you, still not able to get access to KSDK for TWR-K60 board as shown below.

KDS_1.PNG.png

KDS_2.PNG.png

But if we select other board say FRDM-K22 then we have the option to check KSDK as shown min below images.

KDS_2.5.PNG.pngKDS_3.PNG.png

Please help regarding the software, we are planning to use two boards for our RTOS programming project:

  1. TWR-K60D100M: Kinetis K60 100 MHz MCU.
  2. FRDM-KL25Z.

Regards

Abhishek

0 Kudos
Reply