RTCS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,924 Views
netra
Contributor III

How the server will know the client(windows) has shutdown the socket ??

Please reply

0 Kudos
Reply
1 Solution
1,660 Views
butok
NXP Employee
NXP Employee

For UDP server, it should be handled by an application protocol.

For TCP server, the connection is closed automatically, in case of connection graceful shutdown or reset.

If client was physically unplugged and no shutdown was detected by the server, the TCP keep-alive mechanism is used => the connection will be closed in some timeout.

Any manipulations (recv(), send() etc.) with a TCP socket that has closed connection will cause error.

Best regards,

Andrey Butok

View solution in original post

0 Kudos
Reply
1 Reply
1,661 Views
butok
NXP Employee
NXP Employee

For UDP server, it should be handled by an application protocol.

For TCP server, the connection is closed automatically, in case of connection graceful shutdown or reset.

If client was physically unplugged and no shutdown was detected by the server, the TCP keep-alive mechanism is used => the connection will be closed in some timeout.

Any manipulations (recv(), send() etc.) with a TCP socket that has closed connection will cause error.

Best regards,

Andrey Butok

0 Kudos
Reply