RTCS IPv6 gateway

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTCS IPv6 gateway

1,799件の閲覧回数
GudeADS
Contributor III

Hi,

there are functions to access the Ipv4 gateway in RTCS (RTCS_gate_add() ..), but I found no function to get or change the IPv6 (optional RTCS IPv6 stack) gateway address. How can I do this?

Best Regards

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,604件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Andreas,

IPv6 support is available as a separate update package available from Freescale. Visit Internet Protocol for MQX RTOS TCP/IP Stack|NXP

for information on how to evaluate and purchase.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,604件の閲覧回数
GudeADS
Contributor III

Hello soledad,

we bought "1 Year Support & Maint. Renewal for MQX RTOS, Add-on software, IPv6" 6 month ago. So my question stands, I found no function to get or change the IPv6 (optional RTCS IPv6 stack) gateway address. How can I do this?

Best Regards

0 件の賞賛
返信