I am running through the FSL_MQX_in_CW_10_x examples. The hello world example will compile and load in the debugger, but does not run to main. It stops in the bsp where it is checking
while((MCG_S & MCG_S_IREFST_MASK) != 0x00U) { /* Check that the source of the FLL reference clock is the external reference clock. */
}
the new program also gets stuck here and other demos also do not run past this point.
Is there a setting I need to change, or something I need to set in the config.h file. I am using the kinetis K60n512 development board
 
					
				
		
Hi jdwalther,
I suspect problem with jumpers (definitely one related to clock settings - J6). Check the Getting started document to set properly jumpers on your board.
Regards,
MartinK