Question about "virtual_c​om" example in MQX 3.7 & under CW10, twrk60N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about "virtual_c​om" example in MQX 3.7 & under CW10, twrk60N512

ソリューションへジャンプ
1,067件の閲覧回数
anis
Contributor I

Hi,

 

I am using the "virtual_com" example app that comes with MQX 3.7.  I'm running on a twrk60N512 with a Windows/XP PC .

When I run this example - receive  "Unknown (USB) Device" , fsl_ucwxp.inf used.

This result take place  also when, I try start hid_mouse_dev_twrk60n512 example.

When I worked with device from TI( tms320c5505) -  usual driver from MS work properly.

Whether there is a possibility to help with this problem?

  

Thanks,

 Nikolay

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
801件の閲覧回数
JuroV
NXP Employee
NXP Employee

Try to uninstall and install again driver that is determined by the INF file, if it helps.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
802件の閲覧回数
JuroV
NXP Employee
NXP Employee

Try to uninstall and install again driver that is determined by the INF file, if it helps.

0 件の賞賛
返信