Q about MFS limitation on folder depth and number of open files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Q about MFS limitation on folder depth and number of open files

跳至解决方案
2,578 次查看
naftalir
Contributor III

Hi all,

Im having trouble openning few files simultaneously, when there is one file open and im writing into it, and then open a new file and writing to it (using the path: "mfs:folder1/sub_f/file1.001" for file 1, and "mfs:folder2/sub_f/file2.002") i have trouble with it,

getting kernel error uppon address out of scope.

anyone know the probably cause?

Thank you!!

标签 (1)
0 项奖励
回复
1 解答
2,331 次查看
c0170
Senior Contributor III

Hello naftalir,

this might be a problem with TAD. Could you share code snippet?

Regards,

MartinK

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,331 次查看
naftalir
Contributor III

Thanks Kojto,

I dont know what was exactly the error that caused it, but it fixed.. thank you :smileyhappy:

0 项奖励
回复
2,331 次查看
naftalir
Contributor III

P.S: Do i need open multiple mfs instances for each files?

i.e: 1) fopen("mfs1", NULL);

2) fopen("mfs2",NULL);

thanks again...

0 项奖励
回复
2,331 次查看
c0170
Senior Contributor III

Hello naftalir,

can you provide more details, share some code snippet if possible as well, when does the error occur. Sharing details speed up the process to get an answer here :smileywink:

I believe an application does not need to open more instances of MFS to handle more files.

Regards,

MartinK

0 项奖励
回复
2,330 次查看
naftalir
Contributor III

Hi Kojto,

My Scenario is this:

1. install esdhc->sdcard->partition manager->mfs

2. open file in path: "mfs:root1\sub1\file.001"

3. write to file opened above - leave it opened or close it - tried it both scenarios and the results are the same.

4. open new file in path: "mfs:root2\sub1\file.001"

5. Error message: "An Address outside of the KERNEL DATA area wa detected: 0x400b1000" (image attached)

Any clues? :/

Thanks...

0 项奖励
回复
2,332 次查看
c0170
Senior Contributor III

Hello naftalir,

this might be a problem with TAD. Could you share code snippet?

Regards,

MartinK

0 项奖励
回复