Q about MFS limitation on folder depth and number of open files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Q about MFS limitation on folder depth and number of open files

ソリューションへジャンプ
2,679件の閲覧回数
naftalir
Contributor III

Hi all,

Im having trouble openning few files simultaneously, when there is one file open and im writing into it, and then open a new file and writing to it (using the path: "mfs:folder1/sub_f/file1.001" for file 1, and "mfs:folder2/sub_f/file2.002") i have trouble with it,

getting kernel error uppon address out of scope.

anyone know the probably cause?

Thank you!!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,432件の閲覧回数
c0170
Senior Contributor III

Hello naftalir,

this might be a problem with TAD. Could you share code snippet?

Regards,

MartinK

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,432件の閲覧回数
naftalir
Contributor III

Thanks Kojto,

I dont know what was exactly the error that caused it, but it fixed.. thank you :smileyhappy:

0 件の賞賛
返信
2,432件の閲覧回数
naftalir
Contributor III

P.S: Do i need open multiple mfs instances for each files?

i.e: 1) fopen("mfs1", NULL);

2) fopen("mfs2",NULL);

thanks again...

0 件の賞賛
返信
2,432件の閲覧回数
c0170
Senior Contributor III

Hello naftalir,

can you provide more details, share some code snippet if possible as well, when does the error occur. Sharing details speed up the process to get an answer here :smileywink:

I believe an application does not need to open more instances of MFS to handle more files.

Regards,

MartinK

0 件の賞賛
返信
2,431件の閲覧回数
naftalir
Contributor III

Hi Kojto,

My Scenario is this:

1. install esdhc->sdcard->partition manager->mfs

2. open file in path: "mfs:root1\sub1\file.001"

3. write to file opened above - leave it opened or close it - tried it both scenarios and the results are the same.

4. open new file in path: "mfs:root2\sub1\file.001"

5. Error message: "An Address outside of the KERNEL DATA area wa detected: 0x400b1000" (image attached)

Any clues? :/

Thanks...

0 件の賞賛
返信
2,433件の閲覧回数
c0170
Senior Contributor III

Hello naftalir,

this might be a problem with TAD. Could you share code snippet?

Regards,

MartinK

0 件の賞賛
返信