Processor Expert disable ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert disable ?

Jump to solution
2,914 Views
stockfrançois
Contributor I


Hello,

  I have a question about using Processor Expert and MQX_Lite. When I make changes in the processor expert through the component inspector, NO CHANGES will be reported in the code or the architecture of the system.

In the component inspector, It is also writen "Processor Expert disable". What could I do to improve the saving in the PE modifications I have done.

Thanks in advance, have a nice day

Sincerly yours

FRS

PS: I have also posted  the same request in french, if some french-writing people answer, you're welcome

0 Kudos
Reply
1 Solution
2,593 Views
DavidS
NXP Employee
NXP Employee

Hi FRS,

Are you using standalone PE or PE in CW10.4/3/2?

Have you done "Help->Install New Software" to ensure tools are updated?

Is your component enabled? Right click on component and ensure check next to "Component Enabled".

Have you tried to create a new MQXLite project?

Which device are you using?

Regards,

David

View solution in original post

0 Kudos
Reply
2 Replies
2,593 Views
stockfrançois
Contributor I

Hello,

Thanks for quick answering. You're right. I have forgotten to enable the right component in the project explorer panel.

For information, I use a Kinetis MK10DN512ZVLL10 target with a homemade board.

Thanks for all,

Sincerly yours

bye

0 Kudos
Reply
2,594 Views
DavidS
NXP Employee
NXP Employee

Hi FRS,

Are you using standalone PE or PE in CW10.4/3/2?

Have you done "Help->Install New Software" to ensure tools are updated?

Is your component enabled? Right click on component and ensure check next to "Component Enabled".

Have you tried to create a new MQXLite project?

Which device are you using?

Regards,

David

0 Kudos
Reply