Problems jumping from bootloader to application code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems jumping from bootloader to application code

1,544 次查看
dcantero
Contributor II

Hi everybody!!

 

I´m using a MQX program with SD driver and a simple shell as a bootloader in a kinetis K60 tower. The idea is to copy firmware from SD to internal flash and run it.  To test bootloader I have built two projects, first one a "Hello world" example from kinetis software examples (without mqx) and the second one the MQX "Hello World" example. I change the ICF (IAR linker files) in accordance to "Ethernet Bootloader for MCU" application note. Both examples runs OK when debug.

 

When I try to jump from (MQX) bootloader to non MQX "hello world" application everything starts OK until the startup code arrives to "Flash_Identify" function where code access to internal flash. Then the processor resets and the bootloader is executed again. Something similar happends when I trying to jump to a MQX application.

 

I thougth that maybe is necesary to realese some resources in the bootloader before jump. I disbled all interrupts and release some peripherals before jump but the problem remain.

 

Some ideas?. All advices are  wellcome.

 

0 项奖励
回复
1 回复

1,102 次查看
DavidS
NXP Employee
NXP Employee

Did you disable the watchdog timer?

Is the VTOR (vector table) being updated in baremetal and MQX app?

Regards,

David

0 项奖励
回复