Problem with create a task

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with create a task

2,661 次查看
hosseinmoghadda
Contributor III

Hello everybody

I tried to built my custom app by combining GPIO example and throughput demo provided by qualcomm using IAR embedded workbench . You could find second here :   http://www.freescale.com/webapp/connect/displayPartnerProfile.sp?partnerId=5640 

What I changed : 1- clear MQX_AUTO_START_TASK for "WMICONFIG_TASK1" and "WMICONFIG_TASK2" and "SHELL_TASK" in the tasks.c of throughput demo and I add my main task as MQX_AUTO_START_TASK .

Here is my main_task code :

void main_task(uint32_t initial_data){

    /* Structures holding information about specific pin */

    LWGPIO_STRUCT  btn1;

    _task_id wmiconfig1_task_id , wmiconfig2_task_id , shell_task_id ;

    if (!lwgpio_init(&btn1, BSP_BUTTON1, LWGPIO_DIR_INPUT, LWGPIO_VALUE_NOCHANGE))

    {

        printf("Initializing button GPIO as input failed.\n");

        _task_block();

    }

   lwgpio_set_functionality(&btn1, BSP_BUTTON1_MUX_GPIO);

   lwgpio_set_attribute(&btn1, LWGPIO_ATTR_PULL_UP, LWGPIO_AVAL_ENABLE);

   while (TRUE)

   {

   if (LWGPIO_VALUE_LOW == lwgpio_get_value(&btn1)){

   _task_create(0,WMICONFIG_TASK1,0);

   _task_create(0,WMICONFIG_TASK2,0);

   _task_create(0,SHELL_TASK,0);

   if (wmiconfig1_task_id == MQX_NULL_TASK_ID){printf("wmiconfig_task1 can't be created\n");}

   if (wmiconfig2_task_id == MQX_NULL_TASK_ID){printf("wmiconfig_task2 can't be created\n");}

   if (shell_task_id == MQX_NULL_TASK_ID){printf("shell_task can't be created\n");}

   }

}

}

when I load my application to my FRDM_K22F and run it it tells me in the tera term console :

wmiconfig_task1 can't be created

wmiconfig_task2 can't be created

shell_task can't be created

0 项奖励
回复
4 回复数

2,482 次查看
soledad
NXP Employee
NXP Employee

Hello Hossein,

Could you please add the complete project?

Regards

Soledad

0 项奖励
回复

2,482 次查看
hosseinmoghadda
Contributor III

Hello Soledad

You could find my source file here : Dropbox - wmiconfig_qapi.c

Best regards

0 项奖励
回复

2,482 次查看
soledad
NXP Employee
NXP Employee

Hello,

Sorry but I can't  see the TASK_TEMPLATE_STRUCT neither the WMICONFIG_TASK1,WMICONFIG_TASK2,SHELL_TASK functions

Regards

Sol

0 项奖励
回复

2,482 次查看
hosseinmoghadda
Contributor III

Hello

You could find TASK_TEMPLATE_STRUCT here : Dropbox - Tasks.c

WMICONFIG_TASK1 and WMICONFIG_TASK2 here : Dropbox - task_manager.c

and SHELL_TASK here : Dropbox - Shell_Task.c

Best regards

0 项奖励
回复