Problem with RTCS library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with RTCS library

1,797 Views
anthonyboufime
Contributor I

Hello, I am currently working with the FRDM-K64F. For my project I want to run the ethernet functions.

First of all, I worked with the example given in MQX_KSDK like lwip_udpecho or lwip_ping. It worked fine until I try to make my own project.

I followed the structure to instanciate an ethernet connection but I can't find the right library more precisely the .c file. I can include all the file.h but I just have prototypes of functions.

I have also try to use RTCS library but I've got the exact same issues. Indeed, I can include the rtcs.h but it seems there is no rtcs.c.

I've tried to find them in my directories but this file never appear.

How can I find or generate those .c file?

And what is the difference between RTCS and Iwip?

Thanks.

Anthony B.

0 Kudos
Reply
2 Replies

1,609 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Anthony:

I think you can refer the following document, section 5 , building MFS and RTCS library.

http://cache.freescale.com/files/soft_dev_tools/doc/support_info/MQXKSDKGSUG.pdf


Have a great day,
Daniel

0 Kudos
Reply

1,609 Views
towerer
Contributor III

is this still up to date?

with ksdk and processorexpert, i can compile fine using the PE-Module MQX_KSDK. But, this is without RTCS. What is the correct way to implement the rtcs tcpip-stack? I didnt need to build MQX the way it is outlined in that document.... why?

0 Kudos
Reply