Problem with PIT1 interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with PIT1 interrupt

2,725 Views
AF_Ariel
Contributor I

Hello I'm a new mqx user, and i'm working with the MCF52259DEMO Board. I'm looking for some help, with the interruption of the PIT1.
I' need to do a virtual clock (just a simple counter with a variable), but this clock must to be very exact.
So my idea is to make constant interruption with the PIT1 module.
The problem is that I never obtain an interuption, so the code have some kind of problem.
I wrote this code (is very simple), so I'm going to post this:

 

//////this is just the main//////////

 

TASK_TEMPLATE_STRUCT MQX_template_list[] =
{
/*  Task number, Entry point, Stack, Pri, String, Auto? */
   {MAIN_TASK,   Main_task,   5000,  4,   "main", MQX_AUTO_START_TASK,0L,0},
   {0,           0,           0,     0,     0,0,0L,0}
};
extern void dtim3_isr(void);
//////////////////////////////////////////////
//   Clck counter     //
//////////////////////////////////////////////
static unsigned long int clock;
static unsigned int Pit_counter;
//////////////////////////////////////////////////
// Global Register pointer      //
//////////////////////////////////////////////////
VMCF5225_STRUCT_PTR reg_ptr;

/*****************************************************************/
/*****************************************************************/
/*ISR*-----------------------------------------------------------
*
* ISR Name : dtim3_isr

* Comments :

*END*-----------------------------------------------------------*/
__declspec(interrupt)  void dtim3_isr(void)
{
  
   //Set the PIT interrupt flag
   reg_ptr->PIT[1].PCSR=reg_ptr->PIT[1].PCSR;
   // 
   reg_ptr->PIT[1].PMR=Pit_counter;
   /////////////////////////////////////////////////
   //Actualizo el Contador 
   if(clock==1000)
   {
    clock=0;
    reg_ptr->GPIO.PORTTC=reg_ptr->GPIO.PORTTC^0x01;
   }
   else
   {
    clock++;
    reg_ptr->GPIO.PORTTA = reg_ptr->GPIO.PORTTA^0x01;
   }
}


/*****************************************************************/
/*****************************************************************/


/*TASK*-----------------------------------------------------
*
* Task Name    : Main_task
* Comments     :
*    This task prints " Hello World "
*
*END*-----------------------------------------------------*/

void Main_task(uint_32 initial_data)
{

 //////////////////////////////////////////////////////////////
 // Voy a Configurar el IOC0 y el DTIM0 (LED0) like output //
 //////////////////////////////////////////////////////////////
 //First IOC0
 reg_ptr->GPIO.PTAPAR = 0x00;
 reg_ptr->GPIO.DDRTA  = 0x0F;
 reg_ptr->GPIO.PORTTA = 0x00;   
 //Next Led
 reg_ptr->GPIO.PTCPAR = 0x00;
 reg_ptr->GPIO.DDRTC  = 0x0F;
 reg_ptr->GPIO.PORTTC = 0x00;
 //////////////////////////////////////////////////////////////
   
   //PIT1 Init 
 reg_ptr->PIT[1].PCSR=(reg_ptr->PIT[0].PCSR)
 reg_ptr->PIT[1].PMR=reg_ptr->PIT[0].PMR;
 Pit_counter=reg_ptr->PIT[0].PMR;
 
 //Finally Install the PIT1
 if (_int_install_isr(BSP_PIT1_INT_VECTOR,dtim3_isr, NULL) == NULL)
     {
      printf("\n PIT1 instalation fail \n");
     } */
  
 //Init global clock
 clock=0;

     while(1)
     {
     printf("\nTick count =%d\n", clock);
     _time_delay_ticks(200);
     
     }  
}

Please could some body tell me what is the problem?

0 Kudos
Reply
3 Replies

1,655 Views
AF_Ariel
Contributor I

Thank you for your help, now I have the program running well

0 Kudos
Reply

1,655 Views
JuroV
NXP Employee
NXP Employee

Note that your ISR is MQX's kernel ISR, which runs already in interurpt context- so you ISR shoule be __declspec(interrupt) void dtim3_isr(void) only if you are replacing vector in interrupt table. MQX ISR has prototype:

void isr(uint_32 value);

0 Kudos
Reply

1,655 Views
DavidS
NXP Employee
NXP Employee

Hi AF_Ariel,

You had not initialized the reg_ptr correctly.  Also the IMRH bit mask for PIT0 needed to be cleared and lastly the ICR[56] for PIT1 need initialization.

I added you code to my isr.c file that I've hacked up for other test but you should be able to pull out your stuff easily enough.

I've attached my isr.c file.

Happy New Year,

David

0 Kudos
Reply