Problem socket() on mqx3.8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem socket() on mqx3.8

ソリューションへジャンプ
2,190件の閲覧回数
clemNantes
Contributor I

Hi everyone,

 

I have a problem using the socket() function in mqx 3.8 when program pass on this function it look like the processor have interruption pending every-time.

My code :

 

sock_handle = socket(AF_INET, SOCK_STREAM, 0);
                        if(sock_handle == RTCS_SOCKET_ERROR)
                        {
                            printf("socket failed\n\n");
                            //_mqx_exit(0);
                        }else

 

when I execute this code it launch the isr default function of mqx...

Is anyone have an idea? Or the same problem?

I use mqx 3.8 with codewarrior 10.2 on the TWR-K60N512 dev-Kit

 

Best regard,

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,973件の閲覧回数
fcw
Contributor IV

I've found the most typical cause of the default interrupt trap is a stack overflow. I've also found (the hard way) that the yes/no Overflow indication shown in the stack usage MQX RTOS plug-in window isn't always correct. Take a look at task details to make sure.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,974件の閲覧回数
fcw
Contributor IV

I've found the most typical cause of the default interrupt trap is a stack overflow. I've also found (the hard way) that the yes/no Overflow indication shown in the stack usage MQX RTOS plug-in window isn't always correct. Take a look at task details to make sure.

0 件の賞賛
返信
1,973件の閲覧回数
CorderBollie
Contributor II

Shouldn't you use PF_INET (protcol family IP addressing) instead of AF_INET?

0 件の賞賛
返信
1,973件の閲覧回数
butok
NXP Employee
NXP Employee

>>Shouldn't you use PF_INET (protcol family IP addressing) instead of AF_INET?

Eventually, it is the same.

 

Best regards,

Andrey Butok

0 件の賞賛
返信