Problem building MQXLite with GNU Arm Embedded build chain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem building MQXLite with GNU Arm Embedded build chain

Jump to solution
1,987 Views
jwiblin
Contributor II

Hi there.

I am trying to build mqx lite using the GCC arm build chain for a KL25Z target. I am using the processor expert driver suite plugin 10.4 with Eclipse Kepler.

I encounter problems when it comes to building the assembly files. With boot.S i have the followings errors:

'Building file: ../MQXLITE/psp/cortex_m/core/M0/boot.S'

'Invoking: Cross GCC Assembler'

arm-none-eabi-as -I"C:/project/frdm-demo-mqxl/MQXLITE/include" -I"C:/project/frdm-demo-mqxl/MQXLITE/config" -I"C:/project/frdm-demo-mqxl/MQXLITE/kernel" -I"C:/project/frdm-demo-mqxl/MQXLITE/psp/cortex_m" -I"C:/project/frdm-demo-mqxl/MQXLITE/psp/cortex_m/core/M0" -I"C:/project/frdm-demo-mqxl/MQXLITE/psp/cortex_m/compiler/rv" -o "MQXLITE/psp/cortex_m/core/M0/boot.o" "../MQXLITE/psp/cortex_m/core/M0/boot.S"

../MQXLITE/psp/cortex_m/core/M0/boot.S: Assembler messages:

../MQXLITE/psp/cortex_m/core/M0/boot.S:47: Error: bad instruction `asm_comp_specific_directives'

../MQXLITE/psp/cortex_m/core/M0/boot.S:49: Error: unexpected character `t' in type specifier

../MQXLITE/psp/cortex_m/core/M0/boot.S:49: Error: bad instruction `asm_code_section(.text)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:51: Error: bad instruction `set_function_alignment'

../MQXLITE/psp/cortex_m/core/M0/boot.S:53: Error: bad instruction `asm_public(__boot)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:64: Error: bad instruction `asm_equate(NVIC_ICER, 0xE000E180)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:65: Error: bad instruction `asm_equate(NVIC_ICPR, 0xE000E280)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:68: Error: bad instruction `asm_public_begin(__boot)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:69: Error: bad instruction `asm_public_func(__boot)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:70: Error: bad instruction `asm_label(__boot)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:81: Error: selected processor does not support requested special purpose register -- `mrs r0,MSP'

../MQXLITE/psp/cortex_m/core/M0/boot.S:82: Error: selected processor does not support requested special purpose register -- `msr PSP,r0'

../MQXLITE/psp/cortex_m/core/M0/boot.S:85: Error: selected processor does not support requested special purpose register -- `mrs r0,CONTROL'

../MQXLITE/psp/cortex_m/core/M0/boot.S:88: Error: selected processor does not support requested special purpose register -- `msr CONTROL,r0'

../MQXLITE/psp/cortex_m/core/M0/boot.S:94: Error: bad instruction `asm_extern(__thumb_startup)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:95: Error: unrecognized relocation suffix -- `bl ASM_PREFIX(__thumb_startup)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:97: Error: bad instruction `asm_extern(__iar_program_start)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:98: Error: unrecognized relocation suffix -- `bl ASM_PREFIX(__iar_program_start)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:100: Error: bad instruction `asm_extern(__thumb_startup)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:101: Error: unrecognized relocation suffix -- `bl ASM_PREFIX(__thumb_startup)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:103: Error: bad instruction `asm_public_end(__boot)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:106: Error: bad instruction `asm_align(4)'

../MQXLITE/psp/cortex_m/core/M0/boot.S:107: Error: bad instruction `asm_end'

make: *** [MQXLITE/psp/cortex_m/core/M0/boot.o] Error 1

It seems like the assembly instructions used in this file is not compatible with the gcc compiler however it is my understanding that the code generated by the plugin should be compatible with gcc/gnu?

Thanks

James.

0 Kudos
Reply
1 Solution
1,528 Views
jwiblin
Contributor II

I think i might of fixed this. I was setting up the build environment using this tutorial: DIY Free Toolchain for Kinetis: Part 4 – Processor Expert for Eclipse | MCU on Eclipse but when i create a new PEx project and leave the build settings alone it builds fine.

View solution in original post

0 Kudos
Reply
2 Replies
1,528 Views
soledad
NXP Employee
NXP Employee

Hi James,

Thank you for share your solution :smileywink:


Have a great day,
Sol

0 Kudos
Reply
1,529 Views
jwiblin
Contributor II

I think i might of fixed this. I was setting up the build environment using this tutorial: DIY Free Toolchain for Kinetis: Part 4 – Processor Expert for Eclipse | MCU on Eclipse but when i create a new PEx project and leave the build settings alone it builds fine.

0 Kudos
Reply