PN7462AU - External Pin Interrupt In RTOS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7462AU - External Pin Interrupt In RTOS

6,699 次查看
sachin_singh
Contributor II

Hello EveryOne,

Greetings of the day ...!!!

I am working on the PN7462AU, with "PN7462AU-FW_v05.07.01_Full" firmware from NXP site.

I need to add & develop external (GPIO) interrupt button to handle some event.

It will be great if anyone can help me out for the external GPIO interrupt handling in RTOS with some example.

If is there any sample code or document then please share. Which helps to configure all the parameter and ISR calls.

Looking forward for the kind support & response ... !!!

Kind Regards

7 回复数

6,436 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Sachin:

Please refer to the attached MQX ISR example, it is based on Kinetis.

Regards

Daniel

0 项奖励
回复

6,436 次查看
danielchen
NXP TechSupport
NXP TechSupport
0 项奖励
回复

6,436 次查看
sachin_singh
Contributor II

Hi Kan‌,

Can you help me out with External GPIO interrupt in freeRTOS.
I am using PN7462AU firmware package from NXP (PN7462AU-FW_v05.07.01_Full).

Awaiting for your response ... !!!

Thanks

SR

0 项奖励
回复

6,436 次查看
danielchen
NXP TechSupport
NXP TechSupport

I would suggest you refer to below link. A button interrupt task with FreeRTOS was discussed in this thread. Seems similar to what you need.  

Need help with "button" interrupt task (xSemaphoreGiveFromISR) - FreeRTOS 

I hope it helps.

Regards

Daniel

6,436 次查看
sachin_singh
Contributor II

Hi danielchen@fsl‌,

Thanks for your response ...!!! 

I am very grateful to you for supporting interrupt based example in the share link.

I am still developing the code which was mostly looks same.

But, If still I found any issue I will update you for the same.

Regards

SR

0 项奖励
回复

6,436 次查看
sachin_singh
Contributor II

Hi Daniel,

Thanks for document, I will sure look into it.

And I will let you know, If I found any problem into it.

Best Regards

SR  

0 项奖励
回复

6,436 次查看
sachin_singh
Contributor II

Hi Daniel, 

I gone through your attached document and I found that it is for the Kinetis MCU, not for the RTOS.

I am looking for the interrupt sample/example in RTOS for PN7462AU.

RTOS used in PN7462AU is FreeRTOS v9.0.0.

So, If there is any document then please share.

Regards

0 项奖励
回复