PCB-based SPI driver needed for IPC on Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCB-based SPI driver needed for IPC on Kinetis

760 Views
ralphmaas
Contributor I

Hi,

I've developed a solution using the IPC component to connect 2 Kinetis processors using a NULL-modem connection. Now I need to reconfigure this setup to use SPI (one Kinetis in master and the other one in slave mode) and for that I need a PCB-based SPI driver capable of using master and slave mode.

Can anyone tell me if this driver is available and where to find it. If it is nog available (and I have to develop it myself) can anyone direct me to a good starting place for developing PCB-based drivers?

If PCB-based is not really an option I can also develop my own mechanism for the IPC protocol implementation. For that I also need a good starting point.

Can anyone help me to get on track?

Kind regards,

Ralph.

Tags (4)
0 Kudos
Reply
0 Replies