NAND FLASH K70 MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,000件の閲覧回数
Microfelix
Contributor IV

Hello,

in the roadmap of the MQX is written that there would be a driver for NAND FLASH.

I'm using a Kinetis K70, and I would be very glad someone answer me and tell me when there will be a driver for NAND FLASH for MFS MQX.

Maurizio

1 解決策
1,654件の閲覧回数
DavidS
NXP Employee
NXP Employee

Just to update this post.

The FFS is available on the MQX product page download site....just keep clicking the download links (twice...but we are trying to make getting to download page simpler) or click on the below link and find the "Freescale MQX RTOS 4.0.2 FFS package" that has support for K70F120M and K60F120M.

Freescale MQX™ Software Solutions Product Summary Page

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,655件の閲覧回数
DavidS
NXP Employee
NXP Employee

Just to update this post.

The FFS is available on the MQX product page download site....just keep clicking the download links (twice...but we are trying to make getting to download page simpler) or click on the below link and find the "Freescale MQX RTOS 4.0.2 FFS package" that has support for K70F120M and K60F120M.

Freescale MQX™ Software Solutions Product Summary Page

Regards,

David

0 件の賞賛
返信
1,654件の閲覧回数
c0170
Senior Contributor III

Hello Maurizio Felicioni,

there exists a thread with the same question, I answered that it has not been published yet neither I am aware of any specific date.

https://community.freescale.com/thread/304345

I'll try to find out more about date. In the meantime, I lock this thread. Follow the post I sent link to :smileywink:

Regards,

MartinK