MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software..

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software..

跳至解决方案
1,875 次查看
dineshsonagra
Contributor III

For our new development, we are planning to use Freescale's Kinetis K60 processor with software development tool as Code Warrior V10.6 and MQX OS V4.2.

With our embedded hardware control card, we want to generate MySQL data record in the control card and to store the same on NAS drive connected with the system. MySQL server will be running on NAS.

We are looking for MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software to generate MySQL data base using our control card.

Our priority is for MySQL database but if the same is not possible with MQX OS then any other suitable SQL type database will also work Ok for our application.

If any one have such product / tool / Utility to work with above requirement, please send contact - technical details for the same.

标签 (1)
0 项奖励
回复
1 解答
1,653 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Denish,

This question was duplicated and answered here: MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's develo...


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,654 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Denish,

This question was duplicated and answered here: MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's develo...


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复