MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software..

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software..

Jump to solution
1,842 Views
dineshsonagra
Contributor III

For our new development, we are planning to use Freescale's Kinetis K60 processor with software development tool as Code Warrior V10.6 and MQX OS V4.2.

With our embedded hardware control card, we want to generate MySQL data record in the control card and to store the same on NAS drive connected with the system. MySQL server will be running on NAS.

We are looking for MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software to generate MySQL data base using our control card.

Our priority is for MySQL database but if the same is not possible with MQX OS then any other suitable SQL type database will also work Ok for our application.

If any one have such product / tool / Utility to work with above requirement, please send contact - technical details for the same.

Labels (1)
0 Kudos
Reply
1 Solution
1,620 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Denish,

This question was duplicated and answered here: MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's develo...


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,621 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Denish,

This question was duplicated and answered here: MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's develo...


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply