MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software..

ソリューションへジャンプ
1,881件の閲覧回数
dineshsonagra
Contributor III

For our new development, we are planning to use Freescale's Kinetis K60 processor with software development tool as Code Warrior V10.6 and MQX OS V4.2.

With our embedded hardware control card, we want to generate MySQL data record in the control card and to store the same on NAS drive connected with the system. MySQL server will be running on NAS.

We are looking for MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's development software to generate MySQL data base using our control card.

Our priority is for MySQL database but if the same is not possible with MQX OS then any other suitable SQL type database will also work Ok for our application.

If any one have such product / tool / Utility to work with above requirement, please send contact - technical details for the same.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,659件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Denish,

This question was duplicated and answered here: MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's develo...


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,660件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Denish,

This question was duplicated and answered here: MySQL Client library / Conversion tool / Utility compatible to use with MQX OS of Freescale's develo...


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信