MQX4.1.1 I2C example program ran into problem,need help.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX4.1.1 I2C example program ran into problem,need help.

Jump to solution
4,917 Views
tongjianwu
Contributor III

Hello everyone,

When I use the example program for I2C located in <install_dir>\Freescale\Freescale_MQX_4_1\mqx\examples\i2c,I found the program stop at "result = fwrite (mem, 1, 1, fd);"

The E2PROM type is 24C02.

   mem[0] = (uint8_t)addr;

   printf ("  Write to address 0x%02x ... ", mem[0]);

   do

   {

      result = fwrite (mem, 1, 1, fd);

      printf("\r\n Hello World \r\n");

   } while (result < 1)

Need help,thks!

0 Kudos
Reply
1 Solution
4,387 Views
tongjianwu
Contributor III

Hello every one ,

          I have made a mistake,the I2C device address in MQX should be below format:

          for example, AT24C02, addr = 1 0 1 0 A2 A1 A0 R/W,this should be shift right one bit (addr>>1),then this parameter pass to MQX I2C driver .

          Thks !

Best Regards!

View solution in original post

0 Kudos
Reply
8 Replies
4,388 Views
tongjianwu
Contributor III

Hello every one ,

          I have made a mistake,the I2C device address in MQX should be below format:

          for example, AT24C02, addr = 1 0 1 0 A2 A1 A0 R/W,this should be shift right one bit (addr>>1),then this parameter pass to MQX I2C driver .

          Thks !

Best Regards!

0 Kudos
Reply
4,387 Views
poul-erikhansen
Contributor II

I see problems that the driver hangs.
I think it's easiest to modify the polled version.
The drivers in MQX are no specific stable or well written.


Best regards Poul-Erik.



.

0 Kudos
Reply
4,387 Views
tongjianwu
Contributor III

Thks for your reply,

     so what should I do for this problem?

     before that, I test the I2C driver for ACCELEROMETER, the program run normally.

     after that I test the program for my specific E2PROM,I ran into problems.

Best regard

0 Kudos
Reply
4,387 Views
poul-erikhansen
Contributor II

What we have seen is long time stability problems. We use a 24C128 + some IO port expanders, and it works most of the time. I You can't get it working for the first time, You shod use a logic analyzer or a osciloscop.

Best regards.

0 Kudos
Reply
4,387 Views
tongjianwu
Contributor III

Hello,Poul-Erik.

          Can you offer me the E2PROM Demo code?

          Thks!

Best Regards!

0 Kudos
Reply
4,387 Views
tongjianwu
Contributor III

Just now,I test the program for at24c02 and find that " I2C start, send address and get ack ... OK ... ack ==1".

The ACK ought to be '0',now I get ACK=1, I think this is the problem here.

0 Kudos
Reply
4,387 Views
soledad
NXP Employee
NXP Employee

Hello Tong,

Yes you are right, please check the below thread.

[MQX 4.1]I2C demo for MMA8451Q


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,387 Views
tongjianwu
Contributor III

Hello,soledad.

          I have seen the code for ACCELEROMETER and used for TWR_K70F120M,the program run normally,when I use it for E2PROM,there is NACK for sending slave device address byte.

          I use external E2PROM connected to  TWR_K70F120M's I2C0 channel for testing,I don't know why this happen.

          Thks!

Best Regard!

0 Kudos
Reply