MQX4.1.0.1 patch install

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX4.1.0.1 patch install

1,015件の閲覧回数
davidsa
Contributor I

I currently have Freescale_MQX_4_1 and I have tried to install patch MQX4.1.0.1 with the following problems:

C:\Freescale\Freescale_MQX_4_1>patch -p1 --ignore-whitespace -i mqx_4.1.0.1.patc

h

patching file mqx/source/bsp/twrk70f120m/bsp_cm.c

Reversed (or previously applied) patch detected!  Assume -R? [n] R

Apply anyway? [n] Y

Skipping patch.

6 out of 6 hunks ignored -- saving rejects to file mqx/source/bsp/twrk70f120m/bs

p_cm.c.rej

patching file rtcs/source/apps/ftpsrv_task.c

Reversed (or previously applied) patch detected!  Assume -R? [n] Y

Apply anyway? [n] Y

Skipping patch.

1 out of 1 hunk ignored -- saving rejects to file rtcs/source/apps/ftpsrv_task.c

.rej

None of the patches are being updated

0 件の賞賛
返信
1 返信

898件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello David,

I will attend this issue in the thread patch not working for windows 7

Regards

Soledad

0 件の賞賛
返信