MQX4.0 USB-Virtual COM Driver for Win7 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX4.0 USB-Virtual COM Driver for Win7 ?

ソリューションへジャンプ
3,082件の閲覧回数
qianmingzhu
Contributor II

Hi, dear niubility friends !

Here I just run the Virtual COM example which is in MQX4.0 USB device cdc folder.

Above all, everything is fine when I have connected the Virtual COM port to a PC which was installed XP operation system.

Then I changed it to the Win7-64 PC and I found that the inf file, recognized as the driver for XP, was not worked.

Can anybody tell me where to get the driver for Win7-64 OS?

Best wishes for all viewers!

                                                 

                                                                                           Ming

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,117件の閲覧回数
Martin_
NXP Employee
NXP Employee

Try this one, please let us know if it works or not.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,118件の閲覧回数
Martin_
NXP Employee
NXP Employee

Try this one, please let us know if it works or not.

0 件の賞賛
返信
2,117件の閲覧回数
qianmingzhu
Contributor II

Thank godness!

It works!

Best wishes for you Martin!

Thks thks!

0 件の賞賛
返信