MQX4.0 USB-Virtual COM Driver for Win7 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX4.0 USB-Virtual COM Driver for Win7 ?

跳至解决方案
3,083 次查看
qianmingzhu
Contributor II

Hi, dear niubility friends !

Here I just run the Virtual COM example which is in MQX4.0 USB device cdc folder.

Above all, everything is fine when I have connected the Virtual COM port to a PC which was installed XP operation system.

Then I changed it to the Win7-64 PC and I found that the inf file, recognized as the driver for XP, was not worked.

Can anybody tell me where to get the driver for Win7-64 OS?

Best wishes for all viewers!

                                                 

                                                                                           Ming

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,118 次查看
Martin_
NXP Employee
NXP Employee

Try this one, please let us know if it works or not.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,119 次查看
Martin_
NXP Employee
NXP Employee

Try this one, please let us know if it works or not.

0 项奖励
回复
2,118 次查看
qianmingzhu
Contributor II

Thank godness!

It works!

Best wishes for you Martin!

Thks thks!

0 项奖励
回复