MQX4.0 USB-Virtual COM Driver for Win7 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX4.0 USB-Virtual COM Driver for Win7 ?

Jump to solution
3,110 Views
qianmingzhu
Contributor II

Hi, dear niubility friends !

Here I just run the Virtual COM example which is in MQX4.0 USB device cdc folder.

Above all, everything is fine when I have connected the Virtual COM port to a PC which was installed XP operation system.

Then I changed it to the Win7-64 PC and I found that the inf file, recognized as the driver for XP, was not worked.

Can anybody tell me where to get the driver for Win7-64 OS?

Best wishes for all viewers!

                                                 

                                                                                           Ming

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,145 Views
Martin_
NXP Employee
NXP Employee

Try this one, please let us know if it works or not.

View solution in original post

0 Kudos
Reply
2 Replies
2,146 Views
Martin_
NXP Employee
NXP Employee

Try this one, please let us know if it works or not.

0 Kudos
Reply
2,145 Views
qianmingzhu
Contributor II

Thank godness!

It works!

Best wishes for you Martin!

Thks thks!

0 Kudos
Reply