MQX too large, How to shrink the size.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX too large, How to shrink the size.

803 Views
josephgundel
Contributor III

I have ran into an issue using MQX thru KSDK 1.1.0 and KDS 2.0.

The size the OS takes up is unusually large ~ 30K. This is an issue since our chip only has 64K available.

I am just including MQX using processor expert because this is the only way we currently can get it to work.

Any ideas how I can make the MQX footprint smaller? It seems like maybe we are including things we are not using.

Tags (1)
0 Kudos
Reply
1 Reply

726 Views
soledad
NXP Employee
NXP Employee

Hello Joseph,

What device are you using?  Maybe you can use MQXlite.

Regards

Soledad

0 Kudos
Reply