MQX mfs in KSDK 1.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX mfs in KSDK 1.3

1,527 次查看
mscovel
Contributor III

I'm trying to understand how to get MFS/nio to work on an SDHC card in KSDK1.3 (twrk65f180m) in KDS3.2.

I've run the sdcard example which runs but does not seem to recognize commands nor do anything useful.

I've linked in RTCS.

What do I have to do to get MFS started?

What do I have to do to get MFS writing files to the SD card?

What do I have to do to use the MFS API to write files from code/tasks?

4 回复数

1,201 次查看
mscovel
Contributor III

After following the doc above and others as well as the excellent examples, I was able to get RTCS, FTP and MFS running. Kudos to Freescale for making strong software enablement free. I am impressed.

0 项奖励
回复

1,201 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Mark:

Please kindly refer to the below document for add MFS to a MQX RTOS for KSDK project.

https://community.nxp.com/docs/DOC-233598

I hope it is helpful.

Regards

Daniel

0 项奖励
回复

1,201 次查看
mscovel
Contributor III

document you posted isn't there

Thanks

Mark Scovel

260-515-2491

On Fri, Dec 1, 2017 at 12:40 AM, danielchen@fsl <admin@community.nxp.com>

0 项奖励
回复

1,201 次查看
danielchen
NXP TechSupport
NXP TechSupport

Sorry , maybe a typo, please try this link.

https://community.nxp.com/docs/DOC-233598