MQX licensing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX licensing

1,579件の閲覧回数
GottiLuca
Contributor IV

I'd like to publish on GitHub a MQTT implementation based on MQX classic .

Since I'm not a lawyer, I would like to know if there can be some problems with MQX classic ( i.e. : MQX 4.x ) licensing ?

Regards,

Luca

0 件の賞賛
返信
1 返信

1,350件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Luca:

Thank you for checking. The license agreement from NXP only permits distribution of the provided code in object form only, and only if that object code is integrated into a physical device that contains an NXP processor. So this means that the provided NXP code cannot be published online or provided to anyone else electronically regardless of the form it is in (source code, object code, or binary code)

Regards

Daniel

0 件の賞賛
返信