MQX_USE_IO_OLD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX_USE_IO_OLD

2,509件の閲覧回数
arnogir
Senior Contributor II

Hello,

I'm facing some problem on the MFS.

I now update to the MQX 4.2.0.2 to hope to resolve these problem.

During this phase, I seen a parameters : MQX_USE_IO_OLD which is set to 1 into My config.h.

Is anybody can say to me what is exactly the impact of this option?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,421件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

MQX_USE_IO_OLD  set to 1 use the old MQX IO callbacks.

I hope this helps, have a nice day!

Regards

Soledad

0 件の賞賛
返信

2,421件の閲覧回数
arnogir
Senior Contributor II

I see that,

So what is the difference?

I seen inot the mfs for exemple, this use fseek instead another call.

What is the difference in point of view of the user?

0 件の賞賛
返信

2,421件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The following document mentions the changes between MQX version, 

https://www.nxp.com/docs/en/user-guide/MQXCHLGUG.pdf 

please let me know if this helps,

Have a nice day!

Regards

Soledad

0 件の賞賛
返信