MQX: USB CDC Flow Control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX: USB CDC Flow Control

Jump to solution
1,771 Views
huishao2
Contributor IV

Hi-

Is there a way to hold CDC host from sending more data over to device? Basically I am looking for a graceful way of flow control for CDC instead of using blocking API from inside of USB_Notif_Callback().

Thanks and regards

Hui

Labels (1)
0 Kudos
Reply
1 Solution
1,431 Views
soledad
NXP Employee
NXP Employee

Hello Hui,

Please check the below thread, and let me know if this helps

How do I throttle USB device transfers to the device?

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,432 Views
soledad
NXP Employee
NXP Employee

Hello Hui,

Please check the below thread, and let me know if this helps

How do I throttle USB device transfers to the device?

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply