MQX: Stack Ethernet: Send/Received blocked?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX: Stack Ethernet: Send/Received blocked?

跳至解决方案
1,194 次查看
arnogir
Senior Contributor II

Hello

 

I'm using MQX 4.2 on a Kinetis K60.

 

In normal case, all work correctly: Ethernet Modbus is received, managed and response is done.

But sometime, When request is done so fast, at a moment, is blocked. Response is not done to a request, and new request not unblock the recv task.

Bellow is an extract of my code:

 

Initialization in a main task:

/* Allocates resources that RTCS needs and creates TCP/IP task. */ RTCS_create(); /* Read Board ID Number in NV Memory and then Get Mac Address */ ENET_get_mac_address(DV_ETH_ENET_DEVICE, MACLowAddress, DV_Eth_MacAddress); /* Initializes the Ethernet device, adds network interface, and sets up the IPCFG context for it. */ ipcfg_init_device(DV_ETH_ENET_DEVICE, DV_Eth_MacAddress); Error = ipcfg_bind_staticip(DV_ETH_ENET_DEVICE, &DV_Eth_IpData);      DV_Eth_TCPSocketAddr.sin_family       = AF_INET; DV_Eth_TCPSocketAddr.sin_port         = DV_Eth_iGetTCPRxTxPort(); DV_Eth_TCPSocketAddr.sin_addr.s_addr  = INADDR_ANY;  /* Create TCP socket */ DV_Eth_TCPSocketID = socket(PF_INET, SOCK_STREAM, 0); /* Bind TCP socket */ bind(DV_Eth_TCPSocketID, &DV_Eth_TCPSocketAddr, sizeof(DV_Eth_TCPSocketAddr)); /* Listen on TCP port */ listen(DV_Eth_TCPSocketID, 0);  DV_Eth_TCPClientSocketID = accept(DV_Eth_TCPSocketID, &DV_Eth_TCPClientSocketAddr, &DV_Eth_TCPClientSocketAddrLen);   /* Set socket options */ Option = TRUE;      setsockopt(DV_Eth_TCPClientSocketID, SOL_TCP, OPT_SEND_NOWAIT, &Option, sizeof(Option)); setsockopt(DV_Eth_TCPClientSocketID, SOL_TCP, OPT_SEND_PUSH, &Option, sizeof(Option));

 

 

In a receive task, which is always in blocked state and run as soon as satagram is received:

Task: while(1) {  ReadSize = recv(DV_Eth_TCPClientSocketID, BufferPtr, BufferSize, 0);   /* Applciation data managment (Ethernet Modbus) */  Note : This part can call DV_Eth_SendMsg to make a ModBus response  [...] }

 

internal function DV_Eth_SendMsg:

uint32_t DV_Eth_SendMsg(uint8_t *BufferPtr, uint32_t BufferSize) {      int32_t WriteSize = 0;   WriteSize = send(DV_Eth_TCPClientSocketID, BufferPtr, BufferSize, 0);     return((uint32_t)WriteSize); }

 

Bellow is WireShark trace:

Computer is 192.168.1.150

Target Kinetis K60 with MQX is 192.168.1.156

No.     Time                          Source                Destination           Protocol Length Info
Computer done a Modbus request to the target:
15602 2016-03-16 17:22:02.537174    192.168.1.150         192.168.1.156         Modbus/TCP 66        Query: Trans:  3367; Unit:   0, Func:   3: Read Holding Registers
15603 2016-03-16 17:22:02.537504    192.168.1.156         192.168.1.150         TCP      60     502 → 57053 [PSH, ACK] Seq=68344 Ack=56683 Win=3178 Len=0
Target make a response : Ok
15604 2016-03-16 17:22:02.545654    192.168.1.156         192.168.1.150         Modbus/TCP 81     Response: Trans:  3367; Unit:   0, Func:   3: Read Holding Registers
15605 2016-03-16 17:22:02.545747    192.168.1.150         192.168.1.156         TCP      54     57053 → 502 [ACK] Seq=56683 Ack=68371 Win=63492 Len=0
 
 
 
Computer done a Modbus request to the target: 
15606 2016-03-16 17:22:02.583458    192.168.1.150         192.168.1.156         Modbus/TCP 66        Query: Trans:  3367; Unit:   0, Func:   3: Read Holding Registers
15607 2016-03-16 17:22:02.583966    192.168.1.156         192.168.1.150         TCP      60     502 → 57053 [PSH, ACK] Seq=68371 Ack=56695 Win=3166 Len=0
Target ACK the request, but my applciation Recv Task is always blocked necause wait datagram, So No Target response !!!!! NOK !!!!!

Computer done a newly Modbus request to the target:
15608 2016-03-16 17:22:02.619075    192.168.1.150         192.168.1.156         Modbus/TCP 66        Query: Trans:  3367; Unit:   0, Func:   3: Read Holding Registers
15609 2016-03-16 17:22:02.619584    192.168.1.156         192.168.1.150         TCP      60     502 → 57053 [PSH, ACK] Seq=68371 Ack=56707 Win=3154 Len=0
Target ACK the request, but no response
Etc...

In parrallale I have a task which detect cable deconnect:

(simplified code):

 

 

if (ipcfg_get_link_active(DV_ETH_ENET_DEVICE) == FALSE) {  printf("Cable disconnected\n");         printf("\nWaiting for ethernet cable plug in ...\n");  /* Close TCP socket */  DV_Eth_iTCPState = DV_ETH_TCP_WAIT_CONNECT;  DV_Eth_iCloseSocket(DV_Eth_TCPClientSocketID);  ....    if (ipcfg_get_link_active(DV_ETH_ENET_DEVICE) == TRUE)   {   /* Wait new connection */   DV_Eth_TCPClientSocketID = accept(DV_Eth_TCPSocketID, &DV_Eth_TCPClientSocketAddr, &DV_Eth_TCPClientSocketAddrLen);     /* Set socket options */   Option = TRUE;        setsockopt(DV_Eth_TCPClientSocketID, SOL_TCP, OPT_SEND_NOWAIT, &Option, sizeof(Option));   setsockopt(DV_Eth_TCPClientSocketID, SOL_TCP, OPT_SEND_PUSH, &Option, sizeof(Option));  } }

 

 

if I made a cable deconnection/deconnection, socket is reinitialized, but problem still present. Is is mandatory to Reset the µC to make a new MQX init.

 

Is somebody has an Idea, what can I read to try to found where come from my problem? Is any internal MQX status or flag to read can help me to found where the problem come from?

I have a problem in my code?

 

Thank

(Note :   complete source code is provided with this post)

Original Attachment has been moved to: DV_Eth.c.zip

0 项奖励
回复
1 解答
741 次查看
arnogir
Senior Contributor II

Hello

I found the problem

In fact, my modbus application could use some interface via SPI.

Then The SPI access was done via the same file on many task. In my case, one task was preempted by other. twice done SPI access.

When bug occurs, it caused by a task pre empted while SPI communication was in progress and the new task done also an access.

This should cause problem on Interrupt managment and then blocked some action like Ethernet...

:smileydevil:

在原帖中查看解决方案

0 项奖励
回复
1 回复
742 次查看
arnogir
Senior Contributor II

Hello

I found the problem

In fact, my modbus application could use some interface via SPI.

Then The SPI access was done via the same file on many task. In my case, one task was preempted by other. twice done SPI access.

When bug occurs, it caused by a task pre empted while SPI communication was in progress and the new task done also an access.

This should cause problem on Interrupt managment and then blocked some action like Ethernet...

:smileydevil:

0 项奖励
回复