I'm trying to follow the labs that Freescale put out for the TWR-K70. I get stuck at the very beginning because I can't figure out how to create an MQX project in KDS for the TWR-K70.
Can anyone help?
Hello,
KSD supports K70 device, please follow the below steps:
1. Open KDS 3.0
2. Import and MQX example. Go to File->Import a new window will display, select Existing Projects Sets and click next:
3. Select the wsd file for the example code you need, for example I selected "hello", then click open.
4. Build the BSP, PSP libraries and finally the hello example project.
5. In board, check the below jumper configurations:
For standalone operation:
board Rev. B - TWR-K70F120M
• Jumper J18 on position 1-2
• Jumper J19 On
board Rev. C - TWR-K70F120M
• Jumper J18 Off - Y1 Enabled
• Jumper J19 On - Y1 Power
6. Debug the example (select the k70 device used)
As there is not a New MQX 4.2 Project Wizard, it is necessary to create a project from scratch. Please check the below document.
Creating a New MQX RTOS 4.2 project in KDS
Please let me know if this helps!
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------