MQX Serial Driver: the ioctl IO_IOCTL_SERIAL_SET_STOP_BITS is not implemented

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX Serial Driver: the ioctl IO_IOCTL_SERIAL_SET_STOP_BITS is not implemented

跳至解决方案
1,369 次查看
Icenine
Contributor I

Hello!

 

The ioctl IO_IOCTL_SERIAL_SET_STOP_BITS is not implemented for the Kinetis platform.

 

MQX version: 3.7

0 项奖励
回复
1 解答
810 次查看
DavidS
NXP Employee
NXP Employee

Hi Icenine,

The Kinetis SCI modules do not support anything other than 1-bit stop therefore no need to have IOCTL command.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
1 回复
811 次查看
DavidS
NXP Employee
NXP Employee

Hi Icenine,

The Kinetis SCI modules do not support anything other than 1-bit stop therefore no need to have IOCTL command.

Regards,

David

0 项奖励
回复