MQX RTOS cost & licensing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX RTOS cost & licensing

2,297 Views
arifsh10
Contributor I

Hi,

   I am planning to use freescale MCUs in my project.I want MQX RTOS and graphics library to be included with it.I want to know whether MQX rtos is free or we have to purchase it?? I have Kinetis Design studio and Code warrior option for IDE.Is MQX configurable with both of these ? Or any other IDE can be used for MQX ?

0 Kudos
Reply
4 Replies

1,525 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

MQX is free to use on Freescale chips.

Supported IDE includes KDS, codewarrior, IAR, Keil..

Please refer to the following link for details

Freescale MQX™ Software Solutions|Freescale

Regards

Daniel

0 Kudos
Reply

1,525 Views
arifsh10
Contributor I

Thanks for your valuable reply. All features of MQX are free or only basic MQX RTOS is free? I am planning to use Kinetis K series .I need Graphics library and i may need TCP/IP Stack .I MQX rtos is safety certied ? I want to use it in medical equipement.

0 Kudos
Reply

1,525 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

MQX RTOS, TCP/IP (IPv4), usb, MFS, BSP, webserver...is free

MQX add-on software is not free.Please check the following link for details

MQX Add-on Software|Freescale

Regarding the certification, let me check it and get it back to you later

Regards

Daniel

0 Kudos
Reply

1,525 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the following thread for the certification question

Graphics Library and certification of MQX RTOS

Regards

Daniel

0 Kudos
Reply