MQX RTCS demos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX RTCS demos

Jump to solution
2,893 Views
pato3
Contributor III

Running bare-metal on the TWRVF65GS10 with DS-5, most of the MQX 4.0.2 examples are running fine, however for the RTCS eth_to_serial demo, it goes up to "Waiting for  incoming connection..." and then just sits there. IP is configured manually on WIN7 and HyperTerminal returns: "Unable to connect to 192.168.1.202: port 23" and it's the same result with either A5 or M4.

When running httpsrv, I can ping to itself but not to the PC.

Also I followed the "General Technical MQX FAQ" guidelines.

Has anyone managed to get those demos to work on the VF6 without modifications ? with modifications ?

Many thanks in advance

Labels (1)
Tags (2)
1 Solution
2,488 Views
DavidS
NXP Employee
NXP Employee

 

Hi Pato,

I just ran the eth-to-serial demo on my Tower Vybrid kit with TWR-SER card.

 

I had setup my RTOS to use interrupt mode for the UART.  For my Rev F board that is "ittyb".  Your board revision might have a different UART as FYI.

 

I plugged into my home network that also uses 192.168.1. as the gateway/router.  I pinged the 192.168.1.202 to make sure no other device was using it. 

 

Then I ran the eth-to-serial demo and got the following:

 

Waiting for the incoming connection...OK

Then I pinged it from my laptop and got:

Sending ICMP ECHO REQUEST to module

Received ICMP ECHO REPLY

 

Then when I did the connect to the 192.168.1.202:23 the Terminal showed:

Serial <-> Ethernet bridge

And the TCP window showed:

Connecting to 192.168.1.202 ...

Connected to 192.168.1.202

Ethernet <-> Serial bridge

 

If I type something in one window it will show up on the other (unfortunately there was no echo back to the window I type from so that can be confusing).


If you still have issues you might refer to the following Doc Section 7 to make sure your jumpers are configured correctly:

 

C:\Freescale\Freescale_MQX_4_0_2\doc\FSL_MQX_getting_started.pdf


Regards,

David

 

View solution in original post

0 Kudos
Reply
4 Replies
2,489 Views
DavidS
NXP Employee
NXP Employee

 

Hi Pato,

I just ran the eth-to-serial demo on my Tower Vybrid kit with TWR-SER card.

 

I had setup my RTOS to use interrupt mode for the UART.  For my Rev F board that is "ittyb".  Your board revision might have a different UART as FYI.

 

I plugged into my home network that also uses 192.168.1. as the gateway/router.  I pinged the 192.168.1.202 to make sure no other device was using it. 

 

Then I ran the eth-to-serial demo and got the following:

 

Waiting for the incoming connection...OK

Then I pinged it from my laptop and got:

Sending ICMP ECHO REQUEST to module

Received ICMP ECHO REPLY

 

Then when I did the connect to the 192.168.1.202:23 the Terminal showed:

Serial <-> Ethernet bridge

And the TCP window showed:

Connecting to 192.168.1.202 ...

Connected to 192.168.1.202

Ethernet <-> Serial bridge

 

If I type something in one window it will show up on the other (unfortunately there was no echo back to the window I type from so that can be confusing).


If you still have issues you might refer to the following Doc Section 7 to make sure your jumpers are configured correctly:

 

C:\Freescale\Freescale_MQX_4_0_2\doc\FSL_MQX_getting_started.pdf


Regards,

David

 

0 Kudos
Reply
2,488 Views
pato3
Contributor III

Thanks so lot for your reply David, that's all I wanted to know. I don't think it's a big problem, but before starting to dig, I wanted to make sure someone got it working as is with DS-5.

0 Kudos
Reply
2,488 Views
macl
Senior Contributor I

Hi,

Is the IP address on your PC configured to static IP on the same subnet (e.g. 192.168.1.x )?

MacL

0 Kudos
Reply
2,488 Views
pato3
Contributor III

Hi MacL,

Yes it is.

0 Kudos
Reply