MQX Parallel Flash Access issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX Parallel Flash Access issue

1,496 次查看
NSR
Contributor I

Hi All,

We were utilizing the MK60FN1MOVMD12 MCU along with the MQX 3.8 RTOS and the MFS file system, paired with a parallel NOR flash, specifically the Infineon S29GL032N. However, since this NOR flash has become obsolete, we have chosen a new equivalent model with 64MB, identified as Infineon S29GL064S. This new NOR serves as a direct pin-to-pin replacement with the same functionality.
During standard read and write operations, we are encountering an issue where we cannot store data on the flash, and the controller returns an error message stating, 'System encounter database errors! Select OK to format.' We believe this requires modifications in the BSP." But not aware where do to modification.

IS there any one who has come across similar issue or any MQX experts who can put some light on this?

Thanks 

标签 (1)
0 项奖励
回复
1 回复

1,433 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi NSR:

 

I remember there is a MQX BSP porting  guider  under the MQX 4.2 installation folder. You can refer to it .  if you have any question, you can contact the owner of MQX now, embedded access. 

 

 

Regards

Daniel

0 项奖励
回复