MQX + KDS + PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX + KDS + PE

1,829件の閲覧回数
profprogrammer
Contributor III

Hellow.

I am used  Processor Expert in BSP.

When I complying this project.  i get error.

..\Generated_Code\Cpu.c:206:7: error: expected '(' before 'void'

__asm void Cpu_SetBASEPRI(uint32_t Level) {

       ^

11:50:04 Build Finished (took 26s.557ms)

Why there is a mistake?

how to get rid of it?

タグ(1)
0 件の賞賛
返信
1 返信

1,622件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

Could you please specify which MQX version are you using?

Please check the attached document, and try to follow the steps in the page 42.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信