MQX K60 SPI Slow, interrupt mode still calling polled functions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX K60 SPI Slow, interrupt mode still calling polled functions

跳至解决方案
1,213 次查看
shelves
Contributor I

Hi,

 

I'm using the Kinetis Tower K60N512 board. I have run the LTC ADC board examples using the SPI ioctrl command. However, even if you set the mode to be interrupt, the MQX SPI int routine still calls the MQX polled functions for every character. This is slowing my performance.

 

Does anyone have an example of using the interrupt function to just read, or just write. The ioctrl read/write functions are not fast enough for me.

0 项奖励
回复
1 解答
932 次查看
DavidS
NXP Employee
NXP Employee

Hi Shelves,

I updated the MQX3.8/mqx/examples/spi/spic as follows to operate in the either polled (the default setting) or interrupt mode.

    #if ! BSPCFG_ENABLE_SPI2 && ! BSPCFG_ENABLE_ISPI2
        #error This application requires BSPCFG_ENABLE_SPI2 or BSPCFG_ENABLE_ISPI2 defined non-zero in user_config.h. Please recompile kernel with this option.
    #endif
    #if BSPCFG_ENABLE_SPI2
       #define TEST_CHANNEL_POLLED  "spi2:"
 #endif
    #if BSPCFG_ENABLE_ISPI2
        #define TEST_CHANNEL_INT    "ispi2:"
    #endif

 

In my user_config.h I have the following:

#define BSPCFG_ENABLE_ISPI2                       1

 

Always recompiler the RTOS after any change to user_config.h.

 

Please note that IOCTL calls always are accomplished via a polled method.  The inerrupt is used when the fread/fwrite() functions are called.  Please look at the memory_int.c functions as reference.

 

Hope this helps.

Regards,

David

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
933 次查看
DavidS
NXP Employee
NXP Employee

Hi Shelves,

I updated the MQX3.8/mqx/examples/spi/spic as follows to operate in the either polled (the default setting) or interrupt mode.

    #if ! BSPCFG_ENABLE_SPI2 && ! BSPCFG_ENABLE_ISPI2
        #error This application requires BSPCFG_ENABLE_SPI2 or BSPCFG_ENABLE_ISPI2 defined non-zero in user_config.h. Please recompile kernel with this option.
    #endif
    #if BSPCFG_ENABLE_SPI2
       #define TEST_CHANNEL_POLLED  "spi2:"
 #endif
    #if BSPCFG_ENABLE_ISPI2
        #define TEST_CHANNEL_INT    "ispi2:"
    #endif

 

In my user_config.h I have the following:

#define BSPCFG_ENABLE_ISPI2                       1

 

Always recompiler the RTOS after any change to user_config.h.

 

Please note that IOCTL calls always are accomplished via a polled method.  The inerrupt is used when the fread/fwrite() functions are called.  Please look at the memory_int.c functions as reference.

 

Hope this helps.

Regards,

David

 

 

0 项奖励
回复
932 次查看
c0170
Senior Contributor III

Hello shelves,

 

Unfortunately, I have not any example which could help you.  However, this is known issue and SPI driver is going to be redesigned in MQX 4.0.

 

Regards,

MartinK

0 项奖励
回复