MQX GPIO setting quesion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX GPIO setting quesion

ソリューションへジャンプ
3,259件の閲覧回数
miniwang
Contributor III

Hi All,

There is a question about GPIO setting.

I would like to open a gpio file containing pin setting. The code as below. After open the output_set, all of them are set as output, but the pin status only BSP_2972_STANDBY and BSP_2972_RST (D0,D7) are correct. In another words, BSP_9127_RST,BSP_HS_8524_MUTE,BSP_HS_8524_MODE (E24,E25,E26) are set as output LOW.(expect HIGH)

Why I can't control the pin status?

Thank you in advance.

Mini


The environment is [MQX3.8.1] & [CW10.2].

The chip is K20DN512.

-----------------------------------------------------------------------

#define BSP_9127_RST               (GPIO_PORT_E | GPIO_PIN24)   

#define BSP_2972_STANDBY       (GPIO_PORT_D | GPIO_PIN0)

#define BSP_2972_RST               (GPIO_PORT_D | GPIO_PIN7)

#define BSP_HS_8524_MUTE       (GPIO_PORT_E | GPIO_PIN25)

#define BSP_HS_8524_MODE       (GPIO_PORT_E | GPIO_PIN26)

-----------------------------------------------------------------------

    GPIO_PIN_STRUCT output_set[] = {

        BSP_9127_RST              | GPIO_PIN_STATUS_1,

        BSP_2972_STANDBY     | GPIO_PIN_STATUS_0,

        BSP_2972_RST              | GPIO_PIN_STATUS_1,

        BSP_HS_8524_MUTE     | GPIO_PIN_STATUS_1,

        BSP_HS_8524_MODE    | GPIO_PIN_STATUS_1,

        GPIO_LIST_END

    };

    /* Open and set port pins as output */

    output_port = fopen("gpio:write", (char_ptr) &output_set);

    if (NULL == output_port)

    {

        printf("Open to output_port  failed.\n");

    }

-----------------------------------------------------------------------


タグ(1)
1 解決策
2,395件の閲覧回数
miniwang
Contributor III

Thanks Rick,

I can control the pin correct when using "ioctl".  the problem is when I wanna open a gpio file containing pin setting, some of the pins are not correct.

There is a MQX bug I found (For Kinetis). For your reference.

in mqx\source\io\gpio\kgpio\io_gpio_kgpio.c

line number: 322    uint_8    pin;

It should be           uint_32 pin;

cause the width of the GPIO register is 32bits, if give it a byte, only bit 0~7 can work correctly.

that's why some of the pins are correct(D0,D7), and some of them(E24,E25,E26) are not.

元の投稿で解決策を見る

3 返答(返信)
2,395件の閲覧回数
drummer
Contributor IV

you have to issue the ioctl command or nothing gets done

for example: I am multiplexing my analog inputs and need to change the address selector through the GPIO.

uint_32 unc500_scan_vinp(ADC_RESULT_STRUCT * result,uint_8 selector )

{

    ADC_RESULT_STRUCT data;

  uint_32 err;

  if(selector & 1)

  a2d_input_slct[0] |= GPIO_PIN_STATUS_1;

  else

  a2d_input_slct[0] &= ~GPIO_PIN_STATUS_1;

  if(selector & 2)

  a2d_input_slct[1] |= GPIO_PIN_STATUS_1;

  else

  a2d_input_slct[1] &= ~GPIO_PIN_STATUS_1;

  if(selector & 4)

  a2d_input_slct[2] |= GPIO_PIN_STATUS_1;

  else

  a2d_input_slct[2] &= ~GPIO_PIN_STATUS_1;

  ioctl(a2d_selector_fh,GPIO_IOCTL_WRITE, (char_ptr) &a2d_input_slct);

    ioctl(adc8_fh, IOCTL_ADC_FIRE_TRIGGER, (pointer) ADC_TRIGGER_8);

    if (_lwevent_wait_ticks(&evn_vinp,1,TRUE,0) != MQX_OK)

    {

       return FALSE;

    }

    if (_lwevent_clear(&evn_vinp,0x01) != MQX_OK)

    {

       return FALSE;

    }

  err = read(adc8_fh,& data, sizeof(data ));

    result -> result = data.result;

  return err;

}

2,396件の閲覧回数
miniwang
Contributor III

Thanks Rick,

I can control the pin correct when using "ioctl".  the problem is when I wanna open a gpio file containing pin setting, some of the pins are not correct.

There is a MQX bug I found (For Kinetis). For your reference.

in mqx\source\io\gpio\kgpio\io_gpio_kgpio.c

line number: 322    uint_8    pin;

It should be           uint_32 pin;

cause the width of the GPIO register is 32bits, if give it a byte, only bit 0~7 can work correctly.

that's why some of the pins are correct(D0,D7), and some of them(E24,E25,E26) are not.

2,395件の閲覧回数
c0170
Senior Contributor III

Hello Mini Wang,

We will investigate it, however it seems to be obviously incorrectly defined. Thank you for reporting the bug.

Regards,

MartinK

0 件の賞賛
返信