MQX BSP Cloning on CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX BSP Cloning on CodeWarrior

跳至解决方案
1,568 次查看
Fan_xy
Contributor III


hello

I tried cloning a BSP refer to the "MQX-BSP-Cloning-Wizard-Gettiing-Stasrt.pdf"  and I keep always receiving console error messages
when the application tries to Generate MQX Projects (so no proper  cloning done).

The error messages starts with:

111.png

0 项奖励
回复
1 解答
1,329 次查看
RadekS
NXP Employee
NXP Employee

Unfortunately we were not able reproduce it.

Could you please post here whole log (files you can attach in advanced editor – right upper corner of reply window)?

Did you apply bug fix for (globals_full.yml not found)?

https://community.freescale.com/message/431155

Any other changes?


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,330 次查看
RadekS
NXP Employee
NXP Employee

Unfortunately we were not able reproduce it.

Could you please post here whole log (files you can attach in advanced editor – right upper corner of reply window)?

Did you apply bug fix for (globals_full.yml not found)?

https://community.freescale.com/message/431155

Any other changes?


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,329 次查看
jamesmonczynski
Contributor II

I ran into the same problem.

The renaming of the globals.yml to globals_full.yml should fix it.

Let us know if it does.

1,329 次查看
Fan_xy
Contributor III

Yes !