MQX ADC definition errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX ADC definition errors

跳至解决方案
1,229 次查看
ARQuattr
Contributor IV

In adc_k21f.h (in the twrk21f120m bsp with MQX 4.1) there are the following definitions:

#define ADC0_SOURCE_AD4A   (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))
#define ADC0_SOURCE_AD5A   (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))
#define ADC0_SOURCE_AD6A   (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))
#define ADC0_SOURCE_AD7A   (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))

#define ADC1_SOURCE_AD4A   (ADC_SOURCE_MODULE(2) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))
#define ADC1_SOURCE_AD5A   (ADC_SOURCE_MODULE(2) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))
#define ADC1_SOURCE_AD6A   (ADC_SOURCE_MODULE(2) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))
#define ADC1_SOURCE_AD7A   (ADC_SOURCE_MODULE(2) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))

It seems they should be ADC_SOURCE_CHANNEL(4)..(5)..(6)..(7), right?

0 项奖励
回复
1 解答
1,140 次查看
RadekS
NXP Employee
NXP Employee

Yes, it seems that it is a bug.

Thank you for your report.

I will add it to our bug tracking system.


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,141 次查看
RadekS
NXP Employee
NXP Employee

Yes, it seems that it is a bug.

Thank you for your report.

I will add it to our bug tracking system.


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复