MQX 4.2 Missing CodeWarriorNPW folder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX 4.2 Missing CodeWarriorNPW folder

1,416 Views
danir_
Contributor I

Hi,

MQX 4.2 clones correctly with the BSPCloningWizard. But this update losts the reg32 & 64 files & xmls.

It is a bug ?

0 Kudos
Reply
2 Replies

1,256 Views
RadekS
NXP Employee
NXP Employee

Hi Dani,

Thank you for your bug report.

You are right, this feature missing in current version of BSP Cloning Wizard tool.

We changed type of generators (now it is ruby) and we miss this point.

I will report it into our internal bug database.

Note: *.xml and *.reg files are in readable format therefore you can edit them by any text editor.

I generated MY_BOARD411 BSP from frdmk64f BSP. You could take xml file, modify "MY_BOARD411" BSP name into your name and modify MCU type. In reg file you should replace "MY_BOARD411" by your BSP name and edit path to MQX4.2 with MQX version. After that, it should work even with MQX4.2

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,256 Views
danir_
Contributor I

Thanks, I used 4.1.1 files and I updated for 4.2.

0 Kudos
Reply