MQX 4.2 Kinetis websocket behavior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.2 Kinetis websocket behavior

1,029件の閲覧回数
fcw
Contributor IV

I'm intending to use websockets to pass rather long JSON strings to javascript in a browser app. I have things cobbled together and functioning, but it's not a production-ready solution:

-The browser app opens a web socket and sends a message indicating the type of response it is requesting.

- The server message-receive callback builds the response JSON string and attempts to return it via WS_send().

- If the code builds and returns the response from a single large buffer things work as expected.

Given the limited amount of RAM in the K parts, the production code can't afford to statically allocate a large message buffer, allocate it on a stack frame, and certainly will not malloc/free large buffers on a system that needs to remain up and running for unlimited durations.  The attempted solution was to allocate a small buffer, then build the response in chunks and use the FIN flag to indicate end of message as specified by the RTCS user  manual. This completely bolluxes the works:

- WS_send() operations are not sent out the wire until the message-receive callback returns.

- It appears all the chunks are queued and are sent out the wire back to back when the callback returns.

- Re-use of the small buffer for each WS_send() causes the content of each chunk to be the content of the last chunk.

So I would first suggest the behavior of the websocket code needs much better documentation since there's no hint of this in the RTCS 4.2 manual.

Questions:

1. Is there some means to correctly issue multiple WS_send() operations in the context of a message-receive callback?

2. Assuming "No," can multiple WS_send() operations with a small buffer be made to work even outside the context of a message-receive callback? The potential issue I see is the non-blocking behavior of the WS_send() operations inside the receive callback. If the behavior is non-blocking outside the callback, re-writing the buffer will most likely muck up the data sent in earlier calls.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

762件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Fred,

I discussed it with designers and you are right. Web socket implementation is quite complex system which works with pointers instead of simply copying data to send buffer. Also is true that WS_send() operation is non-blocking inside message-receive callback. If WS_send() operation should be blocking inside message-receive callback, this could leads to situations where this task could block himself. So, non-blocking behavior inside message-receive callback is correct behavior and not bug.

So, there should be two general options how to implement such request:

  1. We could use just one WS_send() operations inside message-receive callback. And send next chunk after receive every next answer from browser.
  2. We could use message-receive callback as event and start sending multiple chunks from external place – some different task. In that case, WS_send() operations will be blocking.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信