MQX 4.2 GT202 support patch?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.2 GT202 support patch?

1,270件の閲覧回数
erictexley
Contributor I

Hello to those concerned,

I'm trying to build MQX4.2 with GT202 Atheros support.  I've installed MQX4.2.  I've applied the 4.2.0.2 patch.  I've turned on the BSPCFG_ENABLE_ATHEROS_WIFI as well as BSP_ENET_WIFI_ENABLED.  I've copied the Atheros drivers into the MQX distribution.

When I build, I am getting these errors:

C:/Freescale/Freescale_MQX_4_2/mqx/source/io/enet/atheros_wifi/custom_src/api_interface/cust_api_wmi_rx.c: In function 'fill_scan_info':
C:/Freescale/Freescale_MQX_4_2/mqx/source/io/enet/atheros_wifi/custom_src/api_interface/cust_api_wmi_rx.c:59:16: error: 'ENET_SCAN_INFO' has no member named 'rsn_cipher'
C:/Freescale/Freescale_MQX_4_2/mqx/source/io/enet/atheros_wifi/custom_src/api_interface/cust_api_wmi_rx.c:63:16: error: 'ENET_SCAN_INFO' has no member named 'rsn_cipher'

Am I missing a support patch for MQX4.2 which is required for the GT202 driver?

0 件の賞賛
返信
1 返信

1,084件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Eric:

Unfortunately GT202 is developed by our partner Qaulcomm-Atheros, I would suggest you contact with Qualcomm directly.

However, please check the below thread, in this thread you will find an example of porting the web_hvac demo app to use GT202

https://community.nxp.com/docs/DOC-102702 

I hope it helps

Have a nice day!

Regards

Daniel

0 件の賞賛
返信