Hi,
Now that building MQX 4.1.1 can be easily built using gcc under command line Linux, I would like to build my application/project against MQX 4.1.1. but I don't which startup file to use.
Could you tell me which assembler file generic do I have to compile with my application to run on a K70 or K60, please ?
I have searched for .S files in MQX 4.1.1 directory but I didn not find any of them with a reference to main entry point.
Thank you.
Best regards,
Gaëtan.
Solved! Go to Solution.
 
					
				
		
 Carlos_Musich
		
			Carlos_Musich
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		There are no stupid questions Gaetan, thanks for sharing your findings :smileyhappy:
By the way, you can find boot.S in the following path:
C:\Freescale\Freescale_MQX_4_1\mqx\source\psp\cortex_m\core\M4
Regards,
Carlos
Hi,
I found the solution in MQX_4_1_1_LINUX_GA/demo/hvac/build/make/hvac_twrk70f120m/build_gcc_arm.sh
There is no need of assembly file with main entry point as this belong to MQX core.
Sorry for my stupid question :smileygrin:
Best regards,
Gaëtan?
 
					
				
		
 Carlos_Musich
		
			Carlos_Musich
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		There are no stupid questions Gaetan, thanks for sharing your findings :smileyhappy:
By the way, you can find boot.S in the following path:
C:\Freescale\Freescale_MQX_4_1\mqx\source\psp\cortex_m\core\M4
Regards,
Carlos